Material Declarations
Glossary
ADI F/G Part Number. | The orderable ADI complete exact part number. Example:AD640BP. |
MCV | Maximum concentration value = upper concentration limit, as defined by ADI. |
No Data | Independent lab test results not available. |
Not Used | Not used or contained in the product. |
Package Type | Jedec package designator |
High Temperature Compatible | Compatible at 255+5/-0°C (260°C) peak reflow temperature. |
MSL Rating (per J-STD-020) | Moisture Sensitivity Level rating. |
Peak Reflow Temperature |
Maximum allowable temperature during reflow of component |
RoHs Replacement ADI F/G Part Number |
The orderable RoHS compatible ADI part number for the non RoHS compatible part. |
European Union Exemptions (E) | Parts that have been deemed RoHS compliant and falling under a EU RoHS exemption |
Moisture Sensitivity Level information for legacy Linear products. (PDF)
RoHS Compliance
European Union Directive 2011/65/EC, Restriction of Hazardous Substances (otherwise known as RoHSII), restricts the use of four heavy metals (lead, mercury, cadmium, and hexavalent chromium), and two brominated flame retardants (polybrominated diphenyl ethers and polybrominated biphenyls) in electrical and electronic equipment (EEE) devices. EU Commission published new Directive (EU) 2015/863, amending EU Directive 2011/65/EC, which adds 4 phthalate substances (DEHP, BBP, DBP and DIBP) to the list of 6 already in RoHS II. These 4 phthalate substances will be restricted from use starting July 22, 2019 in most EEE . ADI provides products that allow our customers to be compliant with RoHS regulations. For more information on ADI's RoHS compliance program, see Analog Devices ROHS Compliance Information (pdf).
ADI's RoHS Position Statement (pdf)
Analog Devices evaluation boards are specifically designed for the purpose of research and development and are made available on a business-to-business basis and are therefore excluded from the scope of the RoHS 2 Directive.
EU REACH
REACH is the Regulation (EC) No 1907/2006 of the European Parliament and of the Council of 18 December 2006 concerning the Registration, Evaluation, Authorization and Restriction of Chemicals. It came into force on 1 June 2007. As the REACH List of Substances of Very High Concern (SVHC) is updated by the European Chemicals Agency (ECHA), ADI will provide its customers information regarding its compliance to the current revision of the SVHC list. ADI’s REACH compliance position statement is provided in the link below. For product specific requests for REACH certifications, please contact your regional support center. Please provide your contact information, company and country in your request.
ADI’s EU REACH Position Statementwww.analog.com/en/support/technical-support
Bromine and Chlorine Free
ADI is going beyond RoHS compliance to improve product recyclability by converting to bromine (Br) free and chlorine (Cl) free material sets. Bromine free and chlorine free is also referred to in the industry as halogen free or low halogen. ADI defines halogen free within a homogeneous material to mean the maximum concentration of Br is 900 ppm, the maximum concentration of Cl is 900 ppm, and the maximum concentration of total Br + Cl is 1500 ppm.
All new products are released with halogen free material sets. Customers are notified by PCN for products undergoing conversion to halogen free material sets. ADI is close to completing the transition for lead-framed packages. Nearly all laminate based products are assembled with halogen free die attach adhesives and mold compounds, but older laminate designs might contain bromine and chlorine.
Conflict Minerals
The financial Dodd-Frank Reform Act (Section 1502) requires companies registered on the US Stock Exchange to report and file the use of 3TGs (Tin, Tantalum, Tungsten and Gold) used to manufacture their products. This filing reports whether the sourcing of the 3TGs used had financed or benefited armed groups in the Democratic Republic of Congo or adjoining country.
- Analog Devices (Conflict Mineral Reporting Template)
- Analog Devices' Conflict Mineral Policy
Other Position Statements
- Dimethyl fumarate (“DMF”) Statement (pdf)
- PFOS PFOA Statement (pdf)
- Red Phosphorus Statement (pdf)
- California Proposition 65 Statement (pdf)
- End of Life Vehicle (ELV) Statement (pdf)
- Rare Earth Elements Statement (pdf)
- Toxic Substances Control Act (TSCA) PBT Position Statement (pdf)
For additional information on Analog Devices’ Environmental, Health & Safety Management please visit www.analog.com/en/about-adi/sustainability/environmental-health-safety
Procedure for Return of ADI Evaluation Boards
In accordance with requirements of Waste Electrical and Electronic Equipment – WEEE Directive. This return procedure can be used for evaluation boards containing Pb or RoHS-compliant boards.
- ADI customers in the EU should contact the local sales office to arrange for pick up of evaluation boards for disposal.
- For Eval Board shipments received from a Distributor, customers should return boards to the Distributor directly.
- Evaluation Board WEEE returns should not be mixed with returns of semiconductor components.
- No credits or replacements will be issued.
- ADI will advise customer of the return order number, which customer is asked to reference on the outside of shipping boxes and paperwork.
-
Information that will be required to complete the pick up:
- Date shipment will be ready for collection.
- Number of cartons.
- Weight.
- Contact person & telephone number.
- ADI will forward customer a preprinted waybill which should be handed to the driver on collection, advising them that their local transportation depot will arrange pick up.